How to Achieve Optimal Collimation with Fiber Optics
Collimated light is required for many fiber optic applications. Using the proper setup, fiber optic collimating lenses or ball lenses, and some optical know-how, you can achieve optimal collimation.
Does light entering a multimode fiber undergo a polarization change during propagation through the fiber? If so, can the emerging light be linearly polarized by placing a polarizer at the fiber’s output end?
I would like to view the side profile of a 140μm diameter glass fiber under a microscope. I am having some difficulty resolving the fiber’s border, is there any special lighting technique to use?
Not sure which type of illumination you should use for your system? Learn more about the pros and cons of different illumination types at Edmund Optics.
Choosing the right backlight illumination is critical for precise measurement and edge detection in machine vision applications. Learn about your best options!
Aspherized Achromatic Lenses, exclusive to Edmund Optics, are doublet lenses consisting of two cemented optical elements that are matched for their color-correction ability and small RMS spot size.